STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H755 SDMMC1 with DMA or IT

Hi,I've been trying to get the SDMM1 working on a custom board with an eMMC (ISSI 32GB).Are there any working examples from ST that verifies you have actually tested the MMC side of the HAL library to be working? @Imen DAHMEN​ I am able to get the CS...

TOlli by Senior
  • 2836 Views
  • 4 replies
  • 0 kudos

STM32H743 ADC Conversion/Sampling time

Hi,I wonder if the STM32H743 can sample and convert 1 ADC sample in 10 nanoseconds?According to the specs the ADC speed (sample + convert) at 14bit resolution with 50MHz ADC clock , one sample will take 200 nanoseconds.I have no problem lowering the ...

deckhard by Associate III
  • 1889 Views
  • 5 replies
  • 0 kudos

Callback take long time to trigger

MCU STM32L431, SYSCLK 80MHzThe callback takes 1.5us to fire from pin drop, and the callback functions take long time to execute as I show the imagethe pin config function/** * @brief GPIO Initialization Function * @param None * @retval None */static ...

JSanz.1 by Associate III
  • 2927 Views
  • 5 replies
  • 0 kudos

Resolved! RM0440, Rev 4, STM32G4 Reference Manual - typos

Table 226 on page 906 has an entry HRTIM_TIMxCMP1CR <- I don't think this is a real register.Section 27.3.8, page 888 second line in last paragraph says "any of the 5 timers". I think that should be 6 timers.Section 27.5.66, page 1050 says Bits 31:0 ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.