STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HALL bug not setting clock ?

Hello. I was working on example generated by cubeMX (new version) on STM32L562VET6Q processor and canbus.Example code of networking worked just fine, but copying code to my LL based project made CANBUS inoperable.I was able to track down what is diff...

Linas L by Senior II
  • 1198 Views
  • 1 replies
  • 0 kudos

STM32L0x2 bug in reference manual

RM0376 Reference manual for STM32L0x2 DocID025941 Rev 5 states in 14.9 "Temperature sensor and internal reference voltage" :The following formula gives the actual VDDA voltage supplying the device: VDDA = 3 V x VREFINT_CAL / VREFINT_DATAThis can't be...

MWebj by Associate III
  • 3331 Views
  • 6 replies
  • 0 kudos

Pipeline stage explanation

hi, all. I wanted to ask about The pipeline stages in the m cortex processors , i read that m0 has 3 stages and m0+ has 2 , which renders it more efficient , can anyone explain what that means?

AMat.1 by Associate II
  • 1864 Views
  • 1 replies
  • 0 kudos

F7 UARTs Anything special?

The F4 board worked fine doing UART DMA. I start to regret this upgrade.Forget DMA and IT for now, just trying to get F7 polling working.First HAL_UART_Receive works, but the rest time out.Register analysis is unenlightening going by RM0385 referen...

Sking.21 by Associate III
  • 1897 Views
  • 3 replies
  • 0 kudos

Resolved! STM32L431RC MSI oscillator drift.

I have an application who requires a stable clock source in the whole temperature range but the power budget is tight, so we chose to use the MSI in sync with an external low power 32khz clock.To save extra power we send the core to sleep while it's ...

STM32L5 CANBUS timing setting optimization

Hello. This is my first project with CANBus and i have some questions:I need to interface to motorcycle canbus system, and it is running at 500kbps.All i did is tuned parameters based on scope timings to get 2us/bit. and yes, it did start working, ca...

Linas L by Senior II
  • 900 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.