2020-10-04 10:38 PM
Table 226 on page 906 has an entry HRTIM_TIMxCMP1CR <- I don't think this is a real register.
Section 27.3.8, page 888 second line in last paragraph says "any of the 5 timers". I think that should be 6 timers.
Section 27.5.66, page 1050 says Bits 31:0 Refer to HRTIM_ADC1R bits description <- this should be HRTIM_ADC3R
Section 27.5.67, page 1051 says Bits 31:0 Refer to HRTIM_ADC2R bits description <- this should be HRTIM_ADC4R
Section 27.5.69, page 1055 has a footnote that should be at the end of section 27.5.68, page 1053.
Section 27.5.68, page 1052 bit descriptions call out "ADC trigger 3 ...". If this same description is used for HRTIM_ADC1R, then the trigger number is wrong i.e. it should be "ADC trigger 1 ...".
Section 27.5.69, page 1054 bit descriptions call out "ADC trigger 4 ...". If this same description is used for HRTIM_ADC2R, then the trigger number is wrong i.e. it should be "ADC trigger 2 ...".
Solved! Go to Solution.
2020-10-05 2:33 AM
Hello
Thanks for your contribution.
I will raise your reported case internally to take into consideration.
Imen
2020-10-05 2:33 AM
Hello
Thanks for your contribution.
I will raise your reported case internally to take into consideration.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.