STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Question regarding use of AXIM vs ITCM.

I just solved a bug in my software, and can't quite understand how it happened. My code is a built in hardware test for our board, and a bootloader, which communicates with a serial bus and downloads different compoents to different memories. One o...

SBurc by Associate II
  • 3169 Views
  • 5 replies
  • 0 kudos

how to properly cast ushort to float in Cortex M4 MCU

Hello I have DMA ADC and store data in uint16_t bufferI need to copy these values to input buffer to arm_rfft_fast_f32 function;the function should also cast ushort to float void copy_adc_to_input(uint16_t * int_buff, float32_t * float_buff, uint16_t...

hashtala by Associate II
  • 1827 Views
  • 2 replies
  • 0 kudos

Resolved! Occasional errors on UART's received Bytes.

Hi, everyone,I have been struggling with an issue for sometime. Upon reception, occasionally, a Byte is received with an error in which the most significant bit is received as a '1'. For example, if 0x55 (0101 0101) is sent, 0xD5 (1101 0101) is rece...

PMach.1 by Senior
  • 7039 Views
  • 13 replies
  • 0 kudos

Resolved! Can I use ALL of STM32H750's SRAM for continuous data?

I'm not having any time critical routines so I'm hoping of using all of the MCU's 1MB of RAM for data. As I understand from the RM, RAM is organized in a several banks. Can it be used as a continuous chunk of 1MB for data?

Slina by Associate III
  • 1701 Views
  • 4 replies
  • 0 kudos

CAN ID/MASK Filter Setting

Hi, I am using NUCLEO-F302R8 EV-board. I want to configure the CAN as:use all 3 transmit mailboxes with different mailbox IDFiltering ID number for each mailbox Receive three complete message for each FIFO with filter ID numberBy following CAN settin...

NASI by Senior
  • 1091 Views
  • 0 replies
  • 0 kudos

half-duplex spi slave can't transmit datas

i used stm32f031 as master & slave, NSS is alwasy low, connect MOSI and MISO. the master transmit datas successfull then changing the master direction to receive data( SPI->CR &=~SPI_CR1_BIDIOE), at the same time slave recv and try to transmit data...

Jseyn.1 by Associate III
  • 695 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.