2020-10-03 10:08 PM
Hi,
I am trying to use DMA to realize uncertain length uart message receiving on STM32H745i-DISCO board (on core CM7). My idea is to used IDLE interrupt and then disable the DMA_stream, get the NDTR register and abort the transfer to trigger the DMA TC interrrupt to get the data. I send a string at once, but looks like everytime the IDLE interrupt triggered after receive the first byte. And the the UART_DMAReceiveCplt() function never get chance to be called. Can anyone help me with that?
Thanks!
Solved! Go to Solution.
2020-10-09 12:21 PM
I moved the code from CM7 to CM4, it works. I think it shall be related to DMA_MEM accessibility issue for M7 core. I will try to figure out it by myself.
Also, Tilen Majerle's github repo also used IDLE interrupt instead of RTO interrupt.
2020-10-06 10:39 AM
Can anyone give me some hint what is wrong with my implementation? Thanks!
2020-10-06 1:52 PM
IMHO for this better to use RTO interrupt (RX timeout) rather than IDLE.
Example can be found in Tilen Majerle's github repo.
-- pa
2020-10-09 12:21 PM
I moved the code from CM7 to CM4, it works. I think it shall be related to DMA_MEM accessibility issue for M7 core. I will try to figure out it by myself.
Also, Tilen Majerle's github repo also used IDLE interrupt instead of RTO interrupt.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.