STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CAN is not initialised when RTC enabled

I am designing the application that uses both CAN interface and RTC. I noticed some weired behaviour that I need to fix somehow. Directly after upload the application starts and CAN working properly. With battery present (there is power on VBAT) if I...

RP.2 by Associate
  • 831 Views
  • 0 replies
  • 0 kudos

Low Level I2C readByte out of sync

Hello,I am trying to implement a low level I2C readbyte function, currently trying to read out register 0x41 (TEMP_H) and 0x42 (TEMP_L) from an MPU9250. The issue is that when I debug print the values, it seems that TEMP_H_Buffer appears to have the ...

0693W000004JMIfQAO.png 0693W000004JMIkQAO.png 0693W000004JMIuQAO.png
SVans.1 by Associate
  • 837 Views
  • 0 replies
  • 0 kudos

Resolved! DMA1_Channel7_IRQHandler doesn't get called

HiI am trying to do a simple USART communication via DMA (LL Drivers). I want to send two chars to my STM32F103 from my PC which are received by DMA. In the DMA RX transfer complete callback I want to send some text string, also via DMA back to the s...

0693W000004JLoLQAW.png
PGroe.2 by Associate III
  • 1808 Views
  • 1 replies
  • 0 kudos

use timer to decode pulse/step + direction signal?

STM32 timers can decode quadrature signals.STM32 timers can count external pulses.can STM32 timers do pulse counting AND take counting direction from a second external input?my current solution (on an STM32F303CB/CC, but also F103) is to let the time...

0690X00000AAEraQAH.png
crackwitz by Associate II
  • 1948 Views
  • 2 replies
  • 1 kudos

Problem with USART2 of stm32 f446ze

Hi, I am also new to stm32 micro controllers. I am trying to use UART2 of my microcontroller which is not default(It is not connected with the ST-Link, hence no virtual COM PORT), I am using a USB to TTL connector(TX,RX and GND) for this, I am taking...

MAziz.1 by Associate II
  • 2270 Views
  • 2 replies
  • 0 kudos

Mesure power consumption on STM32H7B3-DK Platform

Hi Team I wanted to measure the power consumed by the device i.e. STM32H7B3I-DK while running any application like taskIs there any api that helps me to measure this can anyone help on finding a way to do this

DRAME.1 by Associate II
  • 1305 Views
  • 2 replies
  • 0 kudos

Resolved! Has the application note AN5419 been released yet?

I want to build a system based on the STM32H735ZGT6. The data sheet (page 115) refers to application note AN5419 "Getting started with STM32H723/733, STM32H725/735 and STM32H730 Value Line hardware development". However, I cannot find it.

Charly by Associate
  • 4884 Views
  • 3 replies
  • 0 kudos

How can i handle two UART ports in one STM32?

Hello,I have questions about handling multiple UART ports.​Connections are;PC <--USB VCP--> STM32(1) <--UART1--> STM32(2) <--UART2--> Target deviceTwo STM32 are both L412K series,And I wanna make a application which forwards data to the target device...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.