STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPUART1 Issue

Hi,I am learning how to use LPUART1 on the Nucleo-64 (STM32L433RCT6P) to generate messages on the COM4 port of my Windows 10 laptop. A "Hello World\r\n" message should be printed every time the blue User Button on the board gets pressed. Here are the...

0693W000005AGrpQAG.png 0693W000005AGruQAG.png 0693W000005AGs4QAG.png
RrW1 by Associate III
  • 4698 Views
  • 12 replies
  • 0 kudos

Resolved! I want to know if I have this right for the STM32 with the HAL library. I have this working on an Atmega. And Arduino has also a lot more examples to find then STM. So due lack of examples I have wrote this.

1) Set output high2) When input is low wait till it is high3) When input is high read 6 characters4) When having read 6 characters then output low and return (or leave while loop)void Get_Instruction(){   HAL_GPIO_WritePin(GPIOA, GPIO_PIN_12, GPI...

Programming Flash without HAL

Hello, I am trying to make my own bootloader for STM32H743AIIx. Unluckly, I can't erase or program flash memory by my code. I unlock both of banks and see LOCK in FLASH_CR goes down. I put PG to up and write data until EOP flag is set. Despite the fa...

Problem with I2S TX / RX Circular DMA on STM32H743ZI2 board

I have a problem with DMA on this board that was not present on an F407 using code generated by Cube.I2S2 has been configured as master half duplex and IS23 as slave half duplex (fed clock and WS of I2S2). The plan was to have a MEMS microphone on th...

JOatl by Associate II
  • 6289 Views
  • 15 replies
  • 0 kudos

ST32H750VB LQFP100 Package for X16 SDRAM usage

Hi,We were planning to use ST32H750VB (LQFP100 Package) in our design. The critical interface in our design will be SDRAM ( planning x16 bit).But while checking pin-multiplexing details for LQFP100 package, we observed that the D[0-15] and A[0-15] ar...

MBair.1 by Associate II
  • 1717 Views
  • 2 replies
  • 0 kudos

Resolved! Lowpower Modes STM32L4 and RTC

Hey there.. iam currently working with a L432KC on a custom made PCB.My programm reads a sensor value (I2C) and sends it so another device via SPI.This operation is performed every minute.iam using the HAL_Delay(60000) command to wait fot the next mi...

MSimo.1 by Associate II
  • 7605 Views
  • 10 replies
  • 0 kudos

STM32F103RB Reset IC neccessary?

I had an issue with a STM32F103RB connected to a poor Power Supply with slow Ramp-Up.In this case, the CAN Peripheral was not correctly initialized. After adding an external Voltage supervisor the Issue dissapeared. My question: is it also possible t...

Hi, I am working on Nucleo -L073RZ board for IAP ymodem , referred the IAP example provided by stm for stm32L073 eval board and created the same for the nucleo board and tested .I have ported all the files and it compiled with zero errors .

The nucleo ported project doesn't work , i cant understand what could be the issue . I keep getting verification failed error , HAL_TIMEOUT .The download timeout is 10000U ,changes made to it (50 seconds) how does this impact the code, will it wai...

svii by Associate III
  • 1993 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.