STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Error with pointer to a typedef struct

Hello, I have a problem with a typedef struct.I made a typedef struct :typedef struct BMP280_HandleTypeDef{  uint16_t dig_T1;  int16_t dig_T2;  int16_t dig_T3;} BMP280_HandleTypeDef ;In my function I declare the instance of it :void myfunction{BMP280...

Prisma by Associate II
  • 2472 Views
  • 2 replies
  • 0 kudos

HAL_UART_Receive_IT (&huart3, Rx_data, 4) ?

Dear Members,I have this code :HAL_UART_Receive_IT (&huart3, Rx_data, 4);I tested from RealTerm, it worked but I need to click "send" 4 times,How can I make it only one click for the whole string ?In STM32 side :char Rx_data[10]; char buf2 [] = "123...

STM32F207 RAM Execution

Hello,I'm developing on an STM32F207 and I would like to know what the procedure to execute code from RAM is?I need to modify a couple of sectors of the internal Flash but the F207 does not have banked memory so I would need to execute the flash eras...

Anvi by Associate III
  • 1657 Views
  • 3 replies
  • 0 kudos

LSI Clock compensation issue, technical datas ?

Hello,I'm working on a low cost design which use LSI Clock. I need to compensate RC osc. deviation as best as possible.I didn't find technical datas about this. Is there any documents with precise datas on deviations according Temp. for examples and ...

F-MA-1 by Associate II
  • 2900 Views
  • 8 replies
  • 0 kudos

STM32L412 interrupt latency and jitter

I am running STM32L412 on 48MHz MSI, Timer 2 is configured in One-Pulse mode to output a 2ms Pulse. This is done by setting Timer 2 in PWM mode and with a prescaler of 47, ARR = 1999 and CCR = 1, Polarity=LOWAn interrupt is generated on update Event,...

0693W000005AHCxQAO.png
b.a. by Associate III
  • 3309 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.