2020-11-06 5:25 AM
Hello, I am trying to make my own bootloader for STM32H743AIIx. Unluckly, I can't erase or program flash memory by my code. I unlock both of banks and see LOCK in FLASH_CR goes down. I put PG to up and write data until EOP flag is set. Despite the fact the full sequence was complete without any errors, I don't see any changes in memory monitor.
2020-11-06 6:12 AM
Also, I have tried to use HAL. It could nor program nor erase too. I used next commands -
HAL_FLASH_Unlock();
FLASH_Erase_Sector(1, FLASH_BANK_1, FLASH_VOLTAGE_RANGE_1);
For erasing value 0x12345678 which was written to 0x0802000 address via memory browser. But nothing happend, the value was unchanged.
2020-11-06 6:55 AM
It helps if you show your actual code.
> For erasing value 0x12345678 which was written to 0x0802000 address via memory browser.
Address 0x0802000 isn't within the flash.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.