STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Phase shifted pwm using stm32f103

I am trying to build a current fed push pull DC DC converter. This requires two waveforms with duty cycle greater than 50% and phase difference of 180 dergrees. I would like to know the possible ways of achieving this. I have tried using output toggl...

MAbba.8 by Associate II
  • 9294 Views
  • 4 replies
  • 0 kudos

Cycle Time

Hey,im going to use the H743 MCU in ~400MHz core frequency with Free Artos operation system.one of my uses is to sample an analog signal with external ADC in SPI Channel.An interrupt to the MCU will inform “samplenow!�?.im trying to figure how much t...

Pkats.1 by Associate II
  • 1344 Views
  • 4 replies
  • 0 kudos

STM32G071 Temperature Sensor stabilization time

HiIn CubeIDE the temperature sensor stabilization time for my STM32G071 is defined by: stm32g0xx_ll_adc.h#define LL_ADC_DELAY_TEMPSENSOR_STAB_US ( 10UL)But in the Datasheet I see at least 15µs max for Tstart(ts_buf) and for Tstart itself its alrea...

0693W000005AhmIQAS.png
PGroe.2 by Associate III
  • 1369 Views
  • 2 replies
  • 0 kudos

interrupt problem

Hi thereI am using a STM32F103C8T6. I defined this pins as External Interrupt:PB4 - GPIO_MODE_IT_RISINGPC13-GPIO_MODE_IT_RISING_FALLINGPC14-GPIO_MODE_IT_RISING_FALLINGPC15-GPIO_MODE_IT_RISING_FALLINGthe problem is that every time I SET/RESET PB4, it ...

Ala by Senior
  • 2235 Views
  • 6 replies
  • 0 kudos

STM32H745 Cortex M7 UART Transmit and Receive with DMA Problem

We have tested UART3 with both Polling and Interrupt and working fine. But now we wanted to receive stream of 25 bytes each line continuously with DMA enable on UART RX.But We are unable to Receive any data with UART DMA. I dont find any example for ...

YSN by Senior
  • 1701 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.