STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is there any required external circuitry for the ADC?

I am using a current sense amplifier (INA190) to measure current. The output of the current sense amplifier will go to the input of the ADC on the STM32. The output range will (ideally) be between (0-VREF). From working with an external 16 bit ADC, I...

JAlle.2 by Associate II
  • 1697 Views
  • 1 replies
  • 0 kudos

STM32F746G-DISCO SDRAM trouble

Hello everyone, I've an STM32F7 Discovery Board. I've been playing with all of the peripherals such a USART, I2C, GPIO, LTDC and SDRAM. And, I've been problems with this last one. I want to do enphasis in that I use to program the device with Atollic...

Jde C.1 by Associate II
  • 2827 Views
  • 6 replies
  • 0 kudos

Calculate number of RTC ticks MCU spends in STOP2 mode

I want to calculate the actual time the CPU spends in STOP2 mode.I wake up the MCU either by RTC Alert or LPUART.The issue is more relevant to LPUART wake use case, because it could happen before the RTC alert expires.I'm using RTC with LSI which con...

deckhard by Associate III
  • 4646 Views
  • 13 replies
  • 0 kudos

Which is the flash configuration of STM32 H7 42 xG ?

Data sheet says: (ch 3.3.1 on page 26)• A user Flash memory block of 512 Kbytes (STM32H7xxxG) or 1-Mbyte (STM32H7xxxI) containing eight user sectors of 128 Kbytes (4 K Flash memory words)which is missing a clear statement for the xxxG variant.Is it f...

HAL_RCC_OscConfig does not return HAL_OK after initializing LSE

Hello,The HAL_RCC_OscConfig does not return HAL_OK after initializing LSE. I tried removing the LSE from Oscillatortype and worked just fine. Also have USART output and clearly it gets stuck at at OSC initialozation.Here is the USART output:[2020-11-...

Kaveh by Associate III
  • 5126 Views
  • 10 replies
  • 0 kudos

Trying to change modes on GPIO pin from input w/EXTI to timer capture. It appears to change modes, but will not capture timer. Any advice?

HAL_GPIO_DeInit(GPIOA, GPIO_PIN_7); //PA7 is no longer GPIO interrupt sourceHere is my code to go into timer mode:/*ReConfigure GPIO pin : PtPin */  GPIO_InitStruct.Pin = Vib_In_Pin;  GPIO_InitStruct.Mode = GPIO_MODE_INPUT;  GPIO_InitStruct.Pull ...

CAnde.1 by Associate
  • 1188 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.