STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have tried a lot of ADC DMA examples, but I don't know where I am failing. I am using a MIKROE card STM32F407VGT6, the result of the DMA register in DataADC comes in only two states (1048 - 0V and 4095 - 3V3)

Here is the code of what i am doing, certainly I am still confused where do I have to change the register. #include "main.h"     /* Private variables ---------------------------------------------------------*/ ADC_HandleTypeDef hadc1; DMA_HandleTypeD...

CSequ.1 by Associate
  • 668 Views
  • 0 replies
  • 0 kudos

Hi, We use a STM32F469 and we would like to add 2x512Mbits of NOR FLASH and 128Mbits of SDRAM. Is ST micro recommand some Part Number for FLASH and SDRAM components ? I have not seen any application note. Thanks

The STM32469I-EVAL has 128Mbits NOR FLASH (PN: S29GL128S90FHI0) and 128 Mbits SDRAM (PN : IS42S32800G-6BLI).There is 512Mbits FLASH version of the S29GL family but the access time is higher. Is it an issue for the STM32F469 ?Which requirements have I...

jtual by Associate II
  • 611 Views
  • 0 replies
  • 0 kudos

strange debug ROM table entries

Hello,I am looking into the ROM tables on STM32F439ZI. TPIU (0xE0040000) class type is 0x9, in its romtable, there are two entries:0xb, which is strange because it is marked as present (0b11) but offset is zero which is prohibited.0x1, which means pr...

mete by Senior II
  • 750 Views
  • 0 replies
  • 0 kudos

Manipulating MCU SPI Interface to Access a Nonstandard SPI

HI There,I want to access multiple SPI slaves at the same time.They all share the same CLK , the same MOSI pin and the same CS.Therefore, I wrote two code sections which basically should do the same.They kind of work, but they both have the same Prob...

TOne.1 by Associate II
  • 2841 Views
  • 8 replies
  • 0 kudos

USART in interrupt mode

Hi, I want to use USART in interrupt mode in stm32f429 evaluation board.I saw the demo example UART_Hyperterminal_IT, but I didn't understood why they are calling HAL_UART_Receive_IT() function if we are using USART in interrupt mode not in polling m...

PNaph.2 by Associate II
  • 1135 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.