2020-11-03 3:46 PM
Hello,
The HAL_RCC_OscConfig does not return HAL_OK after initializing LSE. I tried removing the LSE from Oscillatortype and worked just fine. Also have USART output and clearly it gets stuck at at OSC initialozation.
Here is the USART output:
[2020-11-03_18:06:22:290]Start of program
[2020-11-03_18:06:27:285]------------> 1
[2020-11-03_18:06:27:285]Something went wrong
#include "main.h"
#include "stm32h7xx_hal.h"
#include "string.h"
UART_HandleTypeDef huart2;
TIM_HandleTypeDef htimer2;
uint32_t Input_captures[2] = {0};
uint8_t Count = 1;
uint8_t Is_Capture_Done = FALSE;
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
void GPIO_Init(void);
void TIMER2_Init(void);
void LSE_Config(void);
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim);
char *data = "Hello world, I made it using STM32 ARM Cortex M7!\r\n";
int main(void)
{
HAL_Init();
GPIO_Init();
MX_USART2_UART_Init();
MX_GPIO_Init();
uint8_t Charreceived;
uint8_t Data_Buffer[100];
uint32_t count = 0;
uint8_t Capture_Difference = 0;
double Timer2_CNT_Freq = 0;
double Timer2_CNT_Res = 0;
double User_signal_time_period = 0;
double User_signal_Freq = 0;
char User_msg[100];
data = "Start of program\r\n";
if (HAL_UART_Transmit(&huart2,(uint8_t*)data,strlen(data), HAL_MAX_DELAY) != HAL_OK)
{
// Error occurred
Error_Handler();
}
SystemClock_Config();
TIMER2_Init();
LSE_Config();
while(1)
{
if(Is_Capture_Done)
{
if (Input_captures[1] > Input_captures[0])
Capture_Difference = Input_captures[1] - Input_captures[0];
else
Capture_Difference = (0xFFFFFFFF - Input_captures[0]) + Input_captures[1];
Timer2_CNT_Freq = ((HAL_RCC_GetPCLK1Freq()) / htimer2.Init.Prescaler);
Timer2_CNT_Res = 1 / Timer2_CNT_Freq;
User_signal_time_period = Capture_Difference * Timer2_CNT_Res;
User_signal_Freq = 1 /User_signal_time_period;
}
sprintf(User_msg, "Frequency of the signal applied = %f\r\n", User_signal_Freq);
HAL_UART_Transmit(&huart2, User_msg, strlen(User_msg), HAL_MAX_DELAY);
Is_Capture_Done = FALSE;
//}
data = "---------LOOP\r\n";
//HAL_UART_Transmit(&huart2,(uint8_t*)data,strlen(data), HAL_MAX_DELAY);
}
data = "End of program\r\n";
HAL_UART_Transmit(&huart2,(uint8_t*)data,strlen(data), HAL_MAX_DELAY);
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
//RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI | RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
data = "------------> 1\r\n";
HAL_UART_Transmit(&huart2,(uint8_t*)data,strlen(data), HAL_MAX_DELAY);
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
data = "------------> 2\r\n";
HAL_UART_Transmit(&huart2,(uint8_t*)data,strlen(data), HAL_MAX_DELAY);
Error_Handler();
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USART2;
PeriphClkInitStruct.Usart234578ClockSelection = RCC_USART234578CLKSOURCE_D2PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
data = "------------> 3\r\n";
HAL_UART_Transmit(&huart2,(uint8_t*)data,strlen(data), HAL_MAX_DELAY);
Error_Handler();
}
}
/**
* @brief USART2 Initialization Function
* @param None
* @retval None
*/
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart2, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart2, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
}
void GPIO_Init(void)
{
__HAL_RCC_GPIOD_CLK_ENABLE();
GPIO_InitTypeDef ledgpio;
ledgpio.Pin = GPIO_PIN_14;
ledgpio.Mode = GPIO_MODE_OUTPUT_PP;
ledgpio.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOD, &ledgpio);
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
data = "Something went wrong\r\n";
HAL_UART_Transmit(&huart2,(uint8_t*)data,strlen(data), HAL_MAX_DELAY);
while(1)
{
HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_14);
}
}
void LSE_Config(void)
{
#if 0
RCC_OscInitTypeDef OSC_Init;
// Activating LSE
OSC_Init.OscillatorType = RCC_OSCILLATORTYPE_LSE;
OSC_Init.LSEState = RCC_LSE_ON;
if (HAL_RCC_OscConfig(&OSC_Init) != HAL_OK)
{
Error_Handler();
}
#endif
// Configuring LSE to input pin
HAL_RCC_MCOConfig(RCC_MCO1,RCC_MCO1SOURCE_LSE,RCC_MCODIV_1);
}
void TIMER2_Init(void)
{
TIM_IC_InitTypeDef timer2_IC_Config;
// Initializing Timer
htimer2.Instance = TIM2;
htimer2.Init.CounterMode = TIM_COUNTERMODE_UP;
htimer2.Init.Period = 0xFFFFFFFF;
htimer2.Init.Prescaler = 0x1;
if (HAL_TIM_IC_Init(&htimer2) != HAL_OK)
{
data = "------------> 4\r\n";
HAL_UART_Transmit(&huart2,(uint8_t*)data,strlen(data), HAL_MAX_DELAY);
Error_Handler();
}
// Configuring input channel
timer2_IC_Config.ICFilter = 0;
timer2_IC_Config.ICPolarity = TIM_ICPOLARITY_RISING;
timer2_IC_Config.ICSelection = TIM_ICSELECTION_DIRECTTI;
timer2_IC_Config.ICPrescaler = TIM_ICPSC_DIV1;
if (HAL_TIM_IC_ConfigChannel(&htimer2, &timer2_IC_Config, TIM_CHANNEL_1) != HAL_OK)
{
data = "------------> 5\r\n";
HAL_UART_Transmit(&huart2,(uint8_t*)data,strlen(data), HAL_MAX_DELAY);
Error_Handler();
}
}
void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim)
{
data = "((((((((((((((((((((((((((((((((\r\n";
//HAL_UART_Transmit(&huart2,(uint8_t*)data,strlen(data), HAL_MAX_DELAY);
if(!Is_Capture_Done)
{
data = "*********************************\r\n";
//HAL_UART_Transmit(&huart2,(uint8_t*)data,strlen(data), HAL_MAX_DELAY);
if (Count == 1)
{
Input_captures[0] = __HAL_TIM_GET_COMPARE(htim, TIM_CHANNEL_1);
Count++;
}
else if (Count == 2)
{
Input_captures[1] = __HAL_TIM_GET_COMPARE(htim, TIM_CHANNEL_1);
Is_Capture_Done = TRUE;
Count = 1;
}
}
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
2020-11-03 5:01 PM
Does your board have an LSE? Custom board or an ST board?
2020-11-03 5:12 PM
Yes, it does. It is a custom board.
2020-11-03 6:14 PM
I would attach a debugger, step through the code, and see where it returns. The simplest solution is that the LSE is improperly connected and it times out waiting for the LSE to be enabled. You should also initialize PLL.PLLState = RCC_PLL_NONE, or as appropriate for your configuration.
2020-11-04 5:56 AM
Unfortunately, I don't have any debugger. Any other suggestions?
2020-11-04 6:08 AM
Not really. Debuggers are cheap, so that's what I would do. Check for solder bridges. Use CubeMX generated code to attempt the same thing.
2020-11-04 6:14 AM
Ok. I am new to this. Any suggestion on which debugger?
2020-11-04 6:16 AM
2020-11-04 6:33 AM
I used the USB connection on the board and set it to programming mode by pressing reset & boot buttons. The board does have SDW output and I have a J-link plus available, but never used. Can you please refer me to how to make these 2 work together?
Thanks!
2020-11-17 5:09 PM
Hi TDK,
So the code gets stuck in bellow function inside HAL_RCC_OscConfig / if(((RCC_OscInitStruct->OscillatorType) & RCC_OSCILLATORTYPE_LSE) == RCC_OSCILLATORTYPE_LSE)
while(__HAL_RCC_GET_FLAG(RCC_FLAG_LSERDY) == 0U)
{
if((HAL_GetTick() - tickstart ) > RCC_LSE_TIMEOUT_VALUE)
{
return HAL_TIMEOUT;
}
}
which then calls bellow back and forth
__weak uint32_t HAL_GetTick(void)
{
return uwTick;
}
Any idea what is happening?
Thanks in advance!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.