2020-01-10 4:15 AM
Data sheet says: (ch 3.3.1 on page 26)
• A user Flash memory block of 512 Kbytes (STM32H7xxxG) or 1-Mbyte (STM32H7xxxI)
containing eight user sectors of 128 Kbytes (4 K Flash memory words)
which is missing a clear statement for the xxxG variant.
Is it four sectors of 128kbytes or 8 sectors of 64kbytes?
Thanks a lot
Martin
2020-02-03 6:59 AM
Meanwhile I have xxxG on my hardware and checked it with STLink. That says it has 2M flash.
So it seems it is guaranteed to have four sectors of 128kbytes, maybe it will be 8 sectors.
2020-02-03 8:53 AM
There are a finite set of die being used for these products. Low cost parts being delivered with things turned off, and portions left untested.
The width/size of the flash can depend on the banking options, ie if they have dual banks placed end-to-end, or interleaved side-by-side.
You should check the Option Bytes
2020-02-03 4:33 PM
The "sector" here means erase block, which is always 128 Kbytes (not 64).
The "flash word" here is 32 bytes so 4K "words" is again 128 Kbytes.
-- pa
2020-11-18 3:14 AM
This is still unclear even in the currently available data sheet.
STMs website for STM32H7 says that all STM32H742xG have only 1MB Flash while data sheet stm32h742vg.pdf = DS12110 Rev 7 says on page 54 it is 2MB for I and G versions.
Should be clearla documented
How about the RAM sizes?
Thanks
Martin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.