2020-11-20 7:39 AM
Hi everybody,
With a 4 bits SDIO and stm32f446RE i can read and write data from SD using the FatFs lib, no problem. Ths Sd card is a sanDisk Ultra 8GB (10) MicroSd HC1 class1461. using 512bytes transfers (sector size), the write speed is not so amazing.I bought another card SanDisk 32G MicroSd HC 1 V30 (3) A1 class 3511. Two problems:
1- the software stays stuck in SD init routine, somewhere in GetCmdResp . But when i run the software in debug mode step by step, it is going through. I know timings are longer of course. And when the init has been passed step by step , the software can run freely but the transfer times are higher than the first (10) SD card.
2- Second remark and question, median time is higher but no more peaks ( more that 12ms for a 512bytes write). So time are disappointing.
My main concern is about the step by step to pass the init routines; Any idea why it is acting like that and any solution to go over that issue ? Everyone complains about sdio and HAL and the way ST implemented sdio. Any link on links to working and reliable examples with read:write transfers and SD card management.
Thanks in advance.
pap
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.