STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timing of Hardware Semaphore

We're using a STM32H747IGT6 and using hardware semaphores to coordinate between the two cores.On the CM4 I've set up TIMER3 to run at full blast:  LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_TIM3); LL_TIM_SetPrescaler(TIM3, 0); // Count at sy...

BOOT0 on STM32U083

I have a custom board with an STM32U083KCU6 MCU - see schematics belowVBAT = +3.6VI have 2 boards:1. board: I flashed it via SWD but forgot to enable it in STM32CubeMX, which means that I'm not able to flash it again via SWD2. Board: This time, I rem...

MagnusErler_0-1750599014527.png

On STM32H747IGT6, HSEM channel 0 is reserved?

Application note AN5361 "Setting up with ST-LINK GDB server" says "Set the Cortex®-M7 core running so that the HSEM semaphore is released and Cortex®-M4 wakes up from Stop mode" and this post implies that it's "HSEM 0" which I'm assuming is HSEM chan...

Resolved! STM32U599 OC Tim DMA failed start or do some toggle

We try generate signal defined by toggle table , but command do nothink. (except ARR toggles) if (HAL_TIM_OC_Start_DMA(&htim2, TIM_CHANNEL_4, &tim_values[0], idx) != HAL_OK) { Error_Handler(); }have 1.7.0 U5 firmware some known issue ? O...

MM..1 by Chief III
  • 1438 Views
  • 4 replies
  • 0 kudos

STM32U5 Serial Bootloader AN3155 Discrepancy

In looking at AN3155, USART protocol used in the STM32 bootloader, the following diagram describes the MCU's write protect command sequence from the device side:There is a comment at the bottom which indicates that only certain F and L series chips p...

dsurrett_1-1750720697920.png
dsurrett by Associate II
  • 985 Views
  • 1 replies
  • 0 kudos

MCU Boot Issue - STM32L0

We are using the STM32L071KZU6 in one of our designs and are facing an issue with bootloader communication over I2C. Specifically, some boards fail to enter the bootloader or respond on the I2C bus, while others function normally. Below are the detai...

Resolved! STM32H7 FMC and 16bits device

Hello,I'm kind of newbie in the STM32 world, I'm more used with another brand of 32bits microcontroller that also have a "parrallel port" for interfacing external ram device.My concern is about the FMC on the STM32H7.I want to read/write a 16bits dev...

Alex_J_0-1750105595053.png Alex_J_2-1750105719339.png Alex_J_1-1750105684339.png Alex_J_3-1750105798354.png
Alex_J by Associate II
  • 2418 Views
  • 11 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.