STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 ICs not getting programmed via DFUSE

Hi, we are using STM32H743VIT6 IC for past 3 to 4 years. but from January, none of the newly bought IC is getting programmed via DFUSE. the IC gets connected, erase cycle starts reaches upto 49% and then nothing happens. only the timer is incremented...

dv.13 by Associate II
  • 2422 Views
  • 4 replies
  • 0 kudos

PROBING PINS/LOGICAL ANALYZERS

Hello ST community,I am using STM32L476RG nucleo board and I am interested in reading the boards pin states while running , especially I would like to debug the serial protocols like SPI, I2C, ...I tried with Cube Monitor but it seems, it is only use...

HABIJ.1 by Associate III
  • 1524 Views
  • 4 replies
  • 0 kudos

Double interrupt

I use STM32L552RET.I want to let DMA transfer end interrupt in the 1ms timer interrupt.How to achieve?

XZou.1 by Associate II
  • 648 Views
  • 0 replies
  • 0 kudos

Fastest possible way to receive data from GPIO input

Hello everyone.I want to receive data from AD8283 which is a 12 bit ADC. It has a clock input signal and data will be updated to its 12 bit data signals at each rising edge of clock. For synchronization between ADC and microcontroller I use AD9512 wh...

Resolved! How to generate periodic alarm interrupt from RTC

Hello,I am quite new to STM32G0 based development. I want to generate periodic alarm interrupt from RTC (e.g. RTC should generate an interrupt at every 5 minute, 4 second and 400msec). Is it possible to generate interrupt like this? I tried various w...

HBavi.1 by Associate III
  • 10339 Views
  • 8 replies
  • 0 kudos

I always getting 0xff in my SPI RX Buffer

I used the STM32F401 discovery board which has an L3GD20H gyroscope sensor communicated with the MCU via SPI1, I made the necessary configuration by Cube MXI tried to read the device ID of the gyroscope but each time I received 0xff,can someone help ...

Sdrid.1 by Associate II
  • 2615 Views
  • 4 replies
  • 0 kudos

How to specify RAM location ?

hi, i have an stm32f103 with me ,basically when i run it on keil in simulation mode , i have allotted space in RAM to store variables and data in the picture below ,and although when i look at the address where ram starts at (0x200000000), there is n...

0693W000005CMEEQA4.png 0693W000005CMDuQAO.png
Oahme.1 by Associate III
  • 2079 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.