2020-11-24 1:31 AM
Hello ST community,
I am using STM32L476RG nucleo board and I am interested in reading the boards pin states while running , especially I would like to debug the serial protocols like SPI, I2C, ...
I tried with Cube Monitor but it seems, it is only used to inspect variables and not for probing pins.
Does anyone know if there is a ST tool that can be used for probing pins? If not, could someone recommend a third party tool? I have identified some analogical analyzers that could help : SALEAE, SEGGER J-LINK, ... Does anyone have a user experience to share?
Thanks in advance,
Regards,
2020-11-24 2:16 AM
If you have GPIOx->IDR and ODR in your program, you should be able to read themvia the monitor. I doubt however that you get sensible sampling rates to decode. Saleae works find, if you can couple it to the lines in question.
2020-11-24 2:48 AM
Thanks for the reply,
What do you mean by coupling SALEAE "to the lines in question"?
2020-11-24 5:10 AM
Attach wires to the pins, traces, vias, headers, etc
2020-11-24 5:35 AM
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.