2020-11-24 3:24 AM
Hello everyone.
I want to receive data from AD8283 which is a 12 bit ADC. It has a clock input signal and data will be updated to its 12 bit data signals at each rising edge of clock. For synchronization between ADC and microcontroller I use AD9512 which is a clock distributor and connect one of AD9512 output to one of microcontroller pin. Fastest sample rate for this ADC is 72 MSPS. My question is which microcontroller do you offer to receive its data and how much fast is it?
Which method is faster? Polling microcontroller pin to notify data ready to receive or using parallel-synchronous-transmission-using-gpio-and-dma method?
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.