STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MicroPython .dfu file flashing in NUCLEO-F401RE board

Hi,I want to know procedure to flash latest MicroPython .dfu file in NUCLEO-F401RE board.Please note NUCLEO-F401RE board is having only ST-Link connector. NUCLEO-F401RE board is not having additional USB connector. How to convert .dfu file into .el...

S.Kamath by Associate III
  • 889 Views
  • 0 replies
  • 0 kudos

UART DMA RECEIVE ON STM32H755ZI DUAL-CORE MCU

Hi,Recently I bought a STM32H755ZI Development Board and would like to use it for UART RX with DMA. I used CubeMX to generate the project and everything worked fine with the function "UART_RECEIVE_IT()" but never worked with UART_RECEIVE_DMA(). I've ...

TCHIA by Associate
  • 1830 Views
  • 2 replies
  • 0 kudos

Resolved! I have pruchased a STM32L476VG Discovery board recently. I wanted to build a USB to CAN Interface. For that purpose I need to take CAN Tx, Rx data lines from the STM32 Discovery board and I have to connect those lines to any external transceiver.

I had gone through the datasheet and user manual. I could not fined respective CAN_TX, CAN_RX pins on the board(Pin Number PA12(CAN_TX), PA11(CAN_RX)). These pins are not available on the Discovery board. Then how can I take CAN TX, RX data to the ex...

RahulR by Associate II
  • 1698 Views
  • 2 replies
  • 0 kudos

why external crystal oscillator not working in STM32H7?

Hi,I am using STM32H7 Nucleo board. I soldered an external 25MHz crystal oscillator with 22 pf capacitors(Load capacitance of crystal =20pf) but the controller doesn't seem to work on 25Mhz crystal oscillator. I tested this by blinking an LED at 1 se...

VPras by Associate II
  • 5176 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.