STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have a mono channel to play audio files and can't play stereo files since it allocates more memory. Seems like audio quality of mono file isn't good because I lose a certain part of data.

According to I2S example of STM32373C-EVAL SDK : "Mono audio streaming is not supported (in order to play mono audio streams, each data should be sent twice on the I2S or should be duplicated on the source buffer. Or convert the stream in stereo befo...

Liandri by Associate II
  • 827 Views
  • 0 replies
  • 0 kudos

Level sensitive interrupts with EXTI

I need to achieve level sensitive interrupt behavior with EXTI, similar to shared PCI interrupts on other architectures.Have several OR'ed interrupt requests wired together to a EXTI input;all requests are active low.All requests can be masked or dis...

Pavel A. by Super User
  • 5815 Views
  • 9 replies
  • 0 kudos

STM32L4 RTOS SDCard doesn`t work

Hi, I have custom HW with STM32L496RGTx. On board I have SD card slot. I tried HW with CubeMX. Setted SDMMC1 to Mode: SD 1, SD DMA - SDMMC1 and divider to 24. In code I wroted: FATFS SDFatFs; /* File system object for SD card logical drive */ char S...

lorant124 by Associate III
  • 910 Views
  • 1 replies
  • 0 kudos

Weird characters on I2C 16x2 LCD

Greetings to all.I'm Following some online courses to learn to program STM32. I have a very weird behavior of my board that gives me not few headaches. After reviewing, changing, testing my codes for 2 days i found a way to get my program running cor...

VForm by Associate II
  • 4813 Views
  • 2 replies
  • 0 kudos

Hi, I'm new to STM32L4. I'm trying to connect an ADI evaluation board to my STEVAL-STWIN through SPI2. I had to adapt the different functions to the HAL library.

I am trying to read the register of the chip_id, but the function returns a nDevId that is probably wrong. I set STG3692 switch to obtain SPI configuration and I introduce a GPIO_PIN to configure CS. What could be wrong? below the basicsteps of the c...

GLoiz.1 by Associate
  • 671 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F302R8 TImer 6 Clock Speed / Time BAse

HI,So I cannot seem to get the time base that I expect out of Timer 6. I have got timer working wiht the right freqnecy however I cannot seem to get timer 6 to work at the expected freqency. It seems to be running twice as fast to what I set it to.I ...

glenn0010 by Associate III
  • 3265 Views
  • 6 replies
  • 0 kudos

Resolved! STM32F303CC TIM2 needs a counter overflow before ARR match

Hi and happy new year,Migrating from STM32F103 to STM32F303, I mostly copy&paste my code from STM32103 to STM32F303, and only adjust what's necessary. However, I am having troubles with the TIM2 peripheral. Before starting the counter, the CNT regist...

0693W000006HJV6QAO.png
AAnth.1 by Senior
  • 2395 Views
  • 3 replies
  • 0 kudos

I2C repeated start condition to read BME280 problem

Hi,Device: STM32F103C8T6Driver: LL (low layer)It's been days I have struggle reading BME280 which is connected with i2c to my mcu. After configuration, I'm trying to read registers with standard reading procedure as following:Generate Start condition...

0693W000006HJUXQA4.bmp 0693W000006HJUmQAO.bmp
IDavo.1 by Associate II
  • 706 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.