STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F3 Injected ADC not working on CCR4

Hello I am trying to trigger adc with injected mode using TIM1 CCR 4 event.When i try to use TIM1 upgrade to generate injected ADC interrupt it worked.I used event 0 for adc injected.But when i try to use TIM1 CCR 4 event to trigger injected ADC it i...

Resolved! STM32H7CubeIDE: Is it possible to clone projects?

I have an STM32H735G Discovery Kit and I'm using it with STM32CubeH7 IDE.I want to modify the projects for my own code. Specifically, I want to make a copy of a project.But, I MUST keep the metadata for the toolchain and the debugger. Right now, I ...

DMois.1 by Associate III
  • 2769 Views
  • 7 replies
  • 1 kudos

SPDIFRX_FRAME_SYNC not working/configured?

Hi all,when trying to use the SPDIFRX_FRAME_SYNC on a STM32H743 I ran into a problem.I configure TIM17 as Input capture and set TIM17_TISEL = 1 which should select the SPDIFRX_FRAME_SYNC signal, but the CCR1 register is not updated with the current c...

BKies.1 by Associate
  • 3174 Views
  • 8 replies
  • 2 kudos

Input Trigger capture sources on STM32G4xx

I have an application where I want an external input logic signal to capture a Timer counter value. In my situation the timing measurement is critical so I'm thinking of having the input signal trigger a Timer counter value capture and set a DMA inte...

BTrem.1 by Senior II
  • 1711 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L4xx board has GPIO pin 5 on two different ports (GPIOA and GPIOB) that need to interrupt at different phases of processing. How to initialize PA5 to interrupt initially and the switch to PB5 until done and switch back?

EE designed the board with both pins in use and both needing to wake up from STOP2. At start PA5 must be used to awake. Once awake, switch interrupt to PB5 for normal processing. When normal processing is done, switch back to PA5 and enter STOP2. ...

warm38 by Associate III
  • 2584 Views
  • 4 replies
  • 0 kudos

STMH745 and RTC issue

Hello, I'm using a stm32h745 on my new board with an external 32768Hz quart and setup RTC at startup as follow (using LSE):HalErr_tError HalRtc_Init(void) { HalErr_tError zError = HalErr_eNoError;   /* Configure RTC prescaler and RTC data regis...

DMast.1 by Associate II
  • 1322 Views
  • 1 replies
  • 0 kudos

Faulty pins?

Hey, I made some simple code for my STM32L053C8 Discovery kit to toggle GPIO pins which are connected to LEDs. I used PA0 PA1 and PA2 pins and only PA0 pin responded. Then I turned all GPIO pins high and using LED found some more pins which didn't tu...

DSimp.1 by Associate III
  • 1565 Views
  • 3 replies
  • 1 kudos

STM32F407VG not showing up under my computer

I'm new to STM MCUs and am trying to start with loading basic binary files (mBed) to my STM32F407VG, but when I plug in the MCU it is not appearing in windows file explorer as a drive, which is a problem since I will need to move my binary files ther...

EBroo.1 by Associate II
  • 2301 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.