STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is it possible to run a dual bank flash memory and a SW Watchodg at the same time on stm32F767VI

I am implementing a flash driver on a stm32F767VI. So far the driver works fine until the running with the software watchdog. Of course, the MCU resets on a flash erase to a certain sector.Thanks to the AN4826, I found that I could use the dual bank ...

stm32f407 mem to mem DMA with different Sizes

My data has zeros every 2 bytes.it's like this: 0x55 0x55 00 00 0xaa 0xaa 00 00 0x33 0x33 00 00 ......I want to remove these zeros with address increment feature of DMA.I wrote a configuration for stm32f107 DMA and removed these zeros without problem...

How to calibrate STM32L412 ADC

I have a STM32L412, I am using a 3V external reference but my ADC is not very accurate - it never reaches its full value, even though the voltage present is the same as the external voltage. I want to calibrate the ADC to see if it improves the perfo...

deep_rune by Associate III
  • 1953 Views
  • 2 replies
  • 0 kudos

Resolved! SPI / DMA / D-Cache

HelloI'm confused about SPI in combination with DMA and D-Cache.I'm using the STM32H743ZI and KEIL uVision CMSIS Driver.In my opinion, the CMSIS driver has a weak point. It only sends data by HAL_SPI_TransmitReceive_DMA() if length is a multiple of 3...

Dual core STM32H745, runtime contexts assignment.

For peripheral configuration, CubeMX allows me to assign the same peripheral (ethernet, I2C, etc.) to both Cortex-M7 and Cortex-M4 runtime contexts. Say, for ethernet, what does it mean if i assign the peripheral to both? Since i'm allowed to select...

0693W000006HuzwQAC.png
BVu by Associate III
  • 2658 Views
  • 3 replies
  • 0 kudos

Resolved! Infinite data transmit using SPI

I am testing with STM32F769 Discovery board to make video syncs (not vsync, hsync).I am using SPI module to make infinite clock and data.But, it seems not supported in normal and DMA transmit mode (there is delay between transmissions).How should i ...

SPark.28 by Associate II
  • 1420 Views
  • 2 replies
  • 0 kudos

Resolved! stm32f4xx_it.c overwirtten if I update the configuration

I'm new to STM32 and am trying to get a couple of simple things working at this point. I am trying to generate and handle a GPIO interrupt on PA0 using FreeRTOS and I have no trouble with that. All the examples I've seen say to modify the ISR at st...

JHanc.1 by Associate
  • 2517 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.