2021-01-07 7:11 AM
Hello, I'm using a stm32h745 on my new board with an external 32768Hz quart and setup RTC at startup as follow (using LSE):
HalErr_tError HalRtc_Init(void)
{
HalErr_tError zError = HalErr_eNoError;
/* Configure RTC prescaler and RTC data registers */
/* RTC configured as follows:
- Hour Format = Format 24
- Asynch Prediv = Value according to source clock
- Synch Prediv = Value according to source clock
- OutPut = Output Disable
- OutPutPolarity = High Polarity
- OutPutType = Open Drain */
gRtcHandle.Instance = RTC;
gRtcHandle.Init.HourFormat = RTC_HOURFORMAT_24;
gRtcHandle.Init.AsynchPrediv = RTC_ASYNCH_PREDIV;
gRtcHandle.Init.SynchPrediv = RTC_SYNCH_PREDIV;
gRtcHandle.Init.OutPut = RTC_OUTPUT_DISABLE;
gRtcHandle.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
gRtcHandle.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
if (HAL_RTC_Init(&gRtcHandle) != HAL_OK)
{
/* Initialization Error */
zError = HalErr_eInternal;
}
/** Enable the reference Clock input */
if (HAL_RTCEx_SetRefClock(&gRtcHandle) != HAL_OK)
{
zError = HalErr_eInternal;
}
return zError;
}
void HAL_RTC_MspInit(RTC_HandleTypeDef *hrtc)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;
/*##-1- Enables access to the backup domain ######*/
/* To enable access on RTC registers */
HAL_PWR_EnableBkUpAccess();
/*##-2- Configure LSE/LSI as RTC clock source ###############################*/
#ifdef RTC_CLOCK_SOURCE_LSE
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI | RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.LSIState = RCC_LSI_OFF;
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
while(1){};
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RTC;
PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
if(HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
while(1){};
}
/* Configures the External Low Speed oscillator (LSE) drive capability */
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_HIGH);
#elif defined (RTC_CLOCK_SOURCE_LSI)
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSI | RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.LSEState = RCC_LSE_OFF;
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
while(1){};
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RTC;
PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;
if(HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
while(1){};
}
#else
#error Please select the RTC Clock source inside the main.h file
#endif /*RTC_CLOCK_SOURCE_LSE*/
/*##-3- Enable RTC peripheral Clocks #######################################*/
/* Enable RTC Clock */
__HAL_RCC_RTC_ENABLE();
/*##-4- Configure the NVIC for RTC Alarm ###################################*/
// HAL_NVIC_SetPriority(RTC_Alarm_IRQn, 0x0F, 0);
// HAL_NVIC_EnableIRQ(RTC_Alarm_IRQn);
UNUSED(hrtc);
}I’m experiencing some problems:
1) the clock is always slower (about 10%), no matter of the capacitor installed (even without the capacitors)
2) there is a jitter on the oscillator signal even if the RTC is powered by the Vbat and the uC is not powered
Thanks in advance for any suggestion.
Regards
2021-01-08 11:21 AM
> the clock is always slower
How do you know?
> there is a jitter on the oscillator signal
How do you know?
Read out and check the respective RCC registers whether RTC is properly set to LSE.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.