STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo-H745ZI-Q Serial Comunication and monitoring.

My Nucelo have 4xUART and 4xUSART. How many UART/USART ports can i enable at the same time and how many if any can i monitor on my PC via ST-LINK. Arduino board is really simple you j ust need to chose serial monitor from ArduinoIDE. Is CubeIDE provi...

KBile.1 by Associate II
  • 825 Views
  • 0 replies
  • 0 kudos

Error in smbus clock signal

Hi Team,I am using Smart battery in my product. While reading the battery voltage or current, that value was unexpected. while debugging the clock signal was not correct. In smbus line three devices were connected, Host(mcu (stm32h7)), Master(Battery...

0693W000006IBu5QAG.png
Vel by Associate III
  • 784 Views
  • 0 replies
  • 0 kudos

Resolved! GPIO input maximum frequency

Hello, working with STM32H753 and wanted to know the maximum gpio speed it could achieve. Have achieved only 50MHz using TIM with PWM .Also can it take input of 30MHz 8-bit parallel data? Is there any specific functionality required to achieve high s...

prsh by Associate II
  • 4109 Views
  • 4 replies
  • 0 kudos

How to re-enable the timer after a One pulse goes off (OPM)?

Hi guys I am using the stm32h753zi MCU and writing my own drivers to use the WS2812B led strip.It uses a PWM to determine how much of the RGB you want. I got the PWM part down and the OPM done, the problem is that I want to send let say a duty cycle ...

0693W000006I7vEQAS.png
CLeo.1 by Senior II
  • 2020 Views
  • 9 replies
  • 0 kudos

Resolved! Light up your LED in 30 seconds with 3 methods!

Light up the LED in 30 seconds with 3 methods.​1. Install IDE​Step 0. Prepare HardwareThe hardware used in this experience is ST's development board NUCLEO-F411RE, and the development board number is MB1136. If you don’t have this board, you can use ...

0693W000006H9DbQAK.png 0693W000006H9DMQA0.png 0693W000006H9DvQAK.png 0693W000006H9DlQAK.png
Davis by Associate
  • 2510 Views
  • 2 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.