2021-01-06 1:50 AM
Hello,
I’m currently developping an image software on a nucleo h743zi2 with mbed.
I have to deal with 10b VGA images coming from the DMA & DCMI interface. to store it, I need a RAM bigger than 640 x 480 x 2 bytes = 614.400 bytes.
After looking at th specs of the boad here : i read " Up to 1 Mbyte of RAM: 192 Kbytes of TCM RAM (inc. 64 Kbytes of ITCM RAM + 128 Kbytes of DTCM RAM for time critical routines), Up to 864 Kbytes of user SRAM, and 4 Kbytes of SRAM in Backup domain".
In theory, it is thus ok to store a picture in the user SRAM, with 200kB of extra room for other stuffs.
The issue appears when i try to allocate via a malloc enough space, it crashes.
after some investigation of the memory as mentionned here, it appears that mmy heap is too small (only 497148 bytes).
the issue is still there even when i create a very small program that only print the stack and heap sizes.
it gives me this:
Thread: 0x24004168, Stack size: 516 / 4096
Thread: 0x240041AC, Stack size: 592 / 768
Thread: 0x240041F0, Stack size: 96 / 768
Heap size: 64 / 503316 bytes
The question is thus where are my 300kB of SRAM going ??
Thanks
2021-01-06 6:52 AM
I found the answer:
MEMORY
{
FLASH (rx) : ORIGIN = MBED_APP_START, LENGTH = MBED_APP_SIZE
DTCMRAM (rwx) : ORIGIN = 0x20000298, LENGTH = 128K-0x298
RAM (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
}
The board has 3 separate RAM On different bus and power domains. My program only uses the first one (512k that's why i see +/- 505k of heap in a light program).
As they are not continuous, it is not easily possible to store item larger than 512K... Thus i need another board or smaller frames...
2021-01-06 8:37 AM
You likely want a board with external SDRAM
https://openmv.io/products/openmv-cam-h7-plus
https://www.waveshare.com/product/mcu-tools/core-boards-compact-boards/stm32-core/coreh743i.htm
The heap allocator probably also needs improvement on ST GNU platforms, it has historically been a bit simplistic/sloppy. And where you have different memory classes perhaps an allocation scheme where you pull from an appropriate pool.
2021-01-06 8:50 AM
Thanks i will have a look.
I also found a bigger nucleo with a H7A3ZI. it contains a bank of 1MB RAM (continous this time) but it is not mbed compatible :\
I never understood why ST doesn't add a external RAM on the big nucleo. Such a big processor with no memory is a bit useless in my opinion...
thanks for the help,
2021-01-06 10:08 AM
> I never understood why ST doesn't add a external RAM on the big nucleo.
Nucleos are simple small and cheap (and external memory bus consumes a lot of pins). Consider Discovery boards.
-- pa
2021-01-11 1:38 AM
Check out the Waveshare board
https://www.waveshare.com/product/mcu-tools/core-boards-compact-boards/stm32-core/coreh743i.htm
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.