STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Why do some misaligned operands require more memory cycles than expected to read from the memory of a Cortex-M4?

I wrote some software that reliably measures the number of memory cycles required to retrieve 16 and 32-bit operands from the Cortex-M4 memory. When a 16-bit operand fits within a 32-bit physical word, I would have expected that only a single memory ...

DLewi by Associate II
  • 3442 Views
  • 5 replies
  • 0 kudos

Resolved! UART even parity received WRONG

hey thereI try to receive some characters using UART and here is the confighuart1.Instance = USART1;   huart1.Init.BaudRate = 4800;   huart1.Init.WordLength = UART_WORDLENGTH_8B;   huart1.Init.StopBits = UART_STOPBITS_1;   huart1.Init.Parity = UA...

Ala by Senior
  • 1778 Views
  • 2 replies
  • 0 kudos

How to trigger a function at an output compares ?

Hello,I try that when my OUTPUT compare is triggered, it triggers a function.As for the PeriodElapsedCallback method, when the timer is in overflow, it creates an interuption and the PeriodElapsedCallback function is called. Is there a function doing...

SGROU.1 by Associate III
  • 7126 Views
  • 8 replies
  • 0 kudos

What to change when changing from TIM2 to TIM5?

Hello, I would like to change TIM2 to TIM5 but my code didn't work after I changed that. Could someone help me please? Thanks a lot Here is the code #include "stm32f4xx.h" /* PA0 - TIM2_CH1_ETR/ TIM5_CH1/ TIM8_ETR/ USER BUTTON PA1 - TIM5_CH2/ TIMM2_C...

TrixCZE by Associate II
  • 2370 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F031G6U TIM14 supports OPM (One Pulse Mode)?

STM32CubeMX (STM32Cube_FW_F0_V1.11.2) allows option for One Pulse Mode for TIM14. Does TIM14 actually support OPM on STM32F031G6U? In Reference Manual (RM0091 rev 9), TIM14_CR1 does not have bit 3 OPM. Is mistake in Reference Manual or in STM32CubeMX...

STM32f103c is not detecting in my PC

I had installed required drivers for STM32F103C in my PC and also I had installed necessary packages in keil IDE and Arduino IDE. I am not able find out the problem.I am using ST-Link V2 i have made a proper connection with STM32F103c board.Below I h...

0693W000007CVLCQA4.png 0693W000007CVKdQAO.png
KNesa.1 by Associate
  • 1240 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.