STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SysTick timer registers give an error when called

Hi , i checked the registers for the system clock and i found these registers , but they dont seem to worki , insead , i have to use systick->CTRL , but i cant find the definition from thwere the syntax comes from

0693W000007D2xEQAS.png 0693W000007D2x4QAC.png
AMat.1 by Associate II
  • 719 Views
  • 1 replies
  • 0 kudos

TIMER with DMA call back function

Hi,void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim){ if(htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) {  captureDone = 1; }}HAL_TIM_IC_Start_DMA(&htim2, TIM_CHANNEL_1, (uint32_t*) captures, 2);void HAL_TIM_IC_MspInit(TIM_HandleTypeDef* htim_ic){...

NPULI.1 by Associate II
  • 2194 Views
  • 1 replies
  • 0 kudos

STM32H723 Interface with QuadSPI flash

Hi everyone,for the first time i'm trying to interface my micro H7 to a Macronix QSPI Flash.Micro Model : ST32H723Flash Model : MX25L3233FM1I.These are the instructions that I do:read status register in order to verify QUAD ENABLE (OK)If not QUAD ENA...

MDell.1 by Associate II
  • 2671 Views
  • 0 replies
  • 0 kudos

sprintf function and Cyrillic

I ran into the following problem the sprintf(str, "привет") function; encodes in a two-byte format. Each even character = 208 (dec).str[0] char 208 '�?' str[1] char 159 '\237' str[2] char 209 'Ñ' str[3] char 128 '\200' str[4] char 208 '�?' str[5...

Problem in communicating Modbus with PC

Hi, I am communicating data from Modbus to pc and vice versa using Rs_485 in stm32f103.But I am unable to read and write . I have attached the picture of what error i am getting. can anyone please help me what i need to do. if i need to add ant cod...

Lchal.1 by Associate III
  • 1059 Views
  • 0 replies
  • 0 kudos

Reading from CAN bus (just as plain listener)

Hi ST Experts,Recently I have started with experimentation on STM32407 Discovery board. Basically I am trying to implement CAN bus listener for particular ID from the vehicle. For my testing I am hooking on to OBD (where I have OBD unit to read the ...

PD S.1 by Associate II
  • 6328 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.