2021-01-28 5:12 AM
Hi everyone,
for the first time i'm trying to interface my micro H7 to a Macronix QSPI Flash.
Micro Model : ST32H723
Flash Model : MX25L3233FM1I.
These are the instructions that I do:
All of these instructions are correctly executed.
Then I proceed to write data in Flash (Write enable + 4 x I/O Page Program (4PP))
The problem that I have is that the command 4PP stops after the transmission of 2 bytes of data, with the deactivation of the CHIP SELECT.
What I expected is that with the 4PP command would stop after the transmission of 256 bytes(or at least the number of bytes that I want to transmis, example 8 bytes).
Do you have some suggestion for this ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.