STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to read IC with SMBus interface using I2C?

I want to read registers of BQ40Z50 IC. Its using SMBus for tranceive data. But I need to speak with it using I2C. I use STM32F072 -> I2C2. It doesnt support SMBus-interface, but SMB is based on I2C.I havnt posibility to connect that IC to I2C1. We c...

APoli.1 by Associate
  • 937 Views
  • 0 replies
  • 1 kudos

Main website links broken (403 error)

Hi, From the st.com website/microcontrollers most of the links from the main page result in a "403 error" when clicking on the links to the various micros (See image below)This is an example link that is currently returning a 403 error. Any idea wha...

0690X000006C5bYQAS.jpg

Flash program and erase operations and access latency

Hi,Master:​I have the following questions about flash introduction in the manual (DM00091010):​Question 1:The manual(3.2.2) says:"On the contrary, during a program/erase operation to the Flash memory, any attempt to read the Flash memory will stall t...

Lyu.1 by Senior
  • 920 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H753: How is an ECC in the L1 caches reported

Hi,I'm currently working on a STM32H753. I'm trying to figure out how an ECC error upon a cache look up is reported. The cortex M7 reference manual doesn't provide much info in that regards with the following text:Each cache can also be configured wi...

DBine.1 by Associate
  • 1477 Views
  • 1 replies
  • 0 kudos

Resolved! BSP testing

Hi AlWondering how do you test the infrastructure before delivering it to the application teams?I’m basically referring to the HAL layer , CMSIS and all BSP layer with peripherals.Is there a known methodology for validation tests for these capabiliti...

deckhard by Associate III
  • 1915 Views
  • 3 replies
  • 0 kudos

STM32G070RB, Maximum Alarm length

What is the maximum alarm length in the G070. I only see about 30days.I need 6 months.I guess I could implement one using the TAMP_BKPxR registers and compare the RTC DR , TR with the alarm values I have store in the TAMP regs. ( stripping out the W...

MEder by Associate III
  • 1552 Views
  • 3 replies
  • 0 kudos

STM32H743 Nucleo board SEGGER JLink issue

Hi There, I bought two STM32H743 Nucleo boards recently and did some tests on them. As usual, I first converted ST-Link v2 to JLink interface using the tool SEGGER provided. I have done this with F1, F4, and F7 series boards in order to use JLink RTT...

XZ by Associate II
  • 9472 Views
  • 20 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.