2021-02-12 3:42 AM
We switch several times the µC into Standby Mode and the current is as described in the specification.
But sometimes over the Vdda Pin the current is 1mA.
We switch adc/dac vrefint etc off. No BOR in use.
We checked each Ports, but the current is coming over the VDDA Pin.
What can we check were the current intern the µC flows?
2021-02-12 3:54 AM
Hello..
Vbat measurement (if exists in this model) and temperature measurement probe consume some power when are enabled.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.