STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Confusion with the DBGMCU_IDCODE register.

In our product we will be placing one of 3 different processors. I have developed code to determine this by evaluating the registers for the peripherals, but I'm wondering if there is another way.I've been looking at the DBGMCU_IDCODE register. And o...

mreed by Associate III
  • 6762 Views
  • 6 replies
  • 0 kudos

UART Problem after Flash write

Hi!I'm working in a project that uses flash memory to store calibration data. At the first power on (before writing data in flash) everything works fine. After calibration, if I turn off the board and turn on again, my USART2 stops working (only send...

RBall.1 by Associate
  • 1578 Views
  • 1 replies
  • 0 kudos

STM32H735 SDMMC Error FR_NO_FILESYS

I'm having trouble getting the on board SD card reader working properly. The board is the STM32H735G discovery kit. When attempting to mount the disc it comes back with error FR_NO_FILESYSTEM. A closer investigation shows that when reading the first ...

HSamm.1 by Associate II
  • 3441 Views
  • 5 replies
  • 0 kudos

CAN programming question

Hi !I'm new in the STM32 world ! So, sorry if my questions are stupid. I work on CAN with the example : FDCAN Classic Frame Networking.I want to know if in this example that I modified slightly, HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, TxDa...

KMiko.1 by Associate III
  • 7400 Views
  • 3 replies
  • 0 kudos

How to receive the data from SIM39EA Gps module?

I'm interfacing stm32f series microcontroller and SIM39EA gps module Thruogh terminal im getting this data but not valid data. /**************************************/$GPGSA,A,1,,,,,,,,,,,,,,,*1E$GPGSV,1,1,04,13,,,26,05,,,21,12,,,19,02,,,19*7C$GPRM...

MVENN.1 by Associate II
  • 836 Views
  • 0 replies
  • 0 kudos

STM32F7 How to design external oscillator

Hello,I have been trying for a while now to properly design the external oscillator for the STM32F722RE MCU.Until now, I don't find a clear answer with detail calcul.To design the oscillator, I use 3 documentations:stm32f722re.pdfcd00221665.pdf (AN28...

0693W000007ZLw9QAG.png 0693W000007ZLy0QAG.png 0693W000007ZLrAQAW.png 0693W000007ZLzSQAW.png
BSchn.2 by Associate II
  • 2629 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F373 SDADC Analog input range

Hi, I have 50Hz sinewave with 660mVp-pk, should i connect this to SDADC analog input? It can measure negative cycle of the sinewave? i.e. If i configure SDADC as single ended zero reference mode then it can measure negative cycle of the sinewave?Na...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.