STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! The signal Produced by DAC has errors

Hello,I am building and electric field sensor. The driver signal for it is produced via DAC of the STM32F767zi microcontroller. The signal is 4 kHz and is generated at a sampling speed of 80 kHz via DMA and TIM6. As you can see from the picture the s...

0693W000008wDUqQAM.png
HBesi.1 by Associate II
  • 2643 Views
  • 7 replies
  • 0 kudos

Wakeup from RTC or GPIO not working from Standby

I'm attempting to put my STM32L4xx into Standby mode, and then wake it up from GPIO or RTC. I'm not using any drivers. I've narrowed my problem down to the PWR peripheral clock, although I'm not sure if that is directly the cause. If PWR clock is on ...

DHepp.1 by Associate
  • 2529 Views
  • 3 replies
  • 0 kudos

Resolved! How to update TIM4 PWM duty cycle?

Hello!I have STM32H743BI configure TIM4 to PWM GEnerationstatic void MX_TIM4_Init(void) {   /* USER CODE BEGIN TIM4_Init 0 */   /* USER CODE END TIM4_Init 0 */   TIM_MasterConfigTypeDef sMasterConfig = {0}; TIM_OC_InitTypeDef sConfigOC = {0};...

EEuge by Senior
  • 2496 Views
  • 3 replies
  • 0 kudos

Resolved! RTC, set an alarm for 1 hour in the future.

I want to set a RTC alarm to trigger 1 hour from now but there doesn't seem to be a built-in function (using HAL) to add time. Of course 1 hour in the future is easy unless it happens to be almost midnight or worse almost midnight at the end of the ...

Uart buffer is not resetting to receive new data?

Hello guys, I previously asked the question about the UART interrupt but not get any reply. Currently am able to receive data from uart interrupt but not able to clear the buffer to get new data. please help. my code is void USART1_IRQHandler(void) {...

NHing.1 by Associate III
  • 2208 Views
  • 2 replies
  • 0 kudos

How to enable the cache on the STM32L562-DK in MCUExpresso?

Hi, I am running an application on the STM32L562-DK.  The performance of the application is lower than anticipated.  I started investigating what could be causing the performance issues. I found some example projects that had hal function calls to e...

SSher by Associate II
  • 897 Views
  • 0 replies
  • 0 kudos

How to install stm32 vcp dirver silently, win8,7?

Hi All,I would like to install stm32 vcp dirver (version 1.5.0) silently, without asking any user interaction. I tried to start VCP_V1.5.0_Setup_W8_x64_64bits.exe with \S switch, in this case the installer is started, but it does not finish the proc....

GSzen.1 by Associate
  • 3570 Views
  • 5 replies
  • 0 kudos

Cannot get correct data from MAX31865 SPI bus

Has anybody worked with MAX31865 PT100 sensor chip. I have a module with that chip on a STM32F746 board and SPI bus gives me only zeros. Local loop MOSI->MISO works. The chip doesn't look very complicated but I get nothing out off it. The module has ...

LMI2 by Lead
  • 1981 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.