STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

16 Bit SDADC is only giving 15 Bit value

I am running both SDADCs on a STM32373C-EVAL evaluation board. One of them is giving me the correct values from 0-65.535 but the second one is giving me 0-32.767 on the same voltage.I have configured them using the Cube IDE and Hal. They are set up e...

RKage.3 by Associate
  • 1175 Views
  • 1 replies
  • 0 kudos

Resolved! Fully compatible migration from STM32F745VG to STM32F765VI ?

Hello,For a project I am running code on STM32F745VG. I would like to migrate and replace this MCU with a STM32F765VI with more Flash memory (2MB instead of 1MB). I saw that these two MCUs are pin to pin compatible, but do I need to modify my hardwar...

VPerr.1 by Associate
  • 2258 Views
  • 3 replies
  • 0 kudos

Few questions about STM32 microcontrollers

Hello, I have a few questions about STM32 microcontrollers: I want to create a personalized card and use CAN, RS485, I / O, ... to connect several devicesI need an HMI to control the controller (touchgfx? Or Visual studio?)I want a clear program (mai...

KMiko.1 by Associate III
  • 6498 Views
  • 14 replies
  • 1 kudos

Wake up Pin from standby mode

I am using wake up PIN1 (PA0) to wake the STM32F746 from standby mode. I have PA0 connected to a push button with a pull down resistor. When first powered up the MCU goes into standby mode and stays in it until I press the button connected to PA0. T...

Nano second Precision using a hardware timer on STM32L4S5ZI

Hi,I am working with STM32L4S5ZI MCU and I have a custom board with the same.I am evaluating the hardware timer and as part of my project I need time in nano seconds for some time constrained work. Right now I am using Timer3 and below is my sample c...

SJant.1 by Associate III
  • 7014 Views
  • 17 replies
  • 0 kudos

Resolved! how to jump out of while()?

hey thereI have the code belowuint32_t startTime = HAL_GetTick(); while (HAL_GetTick() - startTime < 5000) { for (int i = 0; i < 3; i++) { if (strstr(InputMSG, answerSearch[i])) { resault = 1; break; } } }wh...

Ala by Senior
  • 1543 Views
  • 2 replies
  • 0 kudos

Resolved! STM32G0B1 release date and compatibility

HiCurrently we are using the STM32G071 MCU, but we will running out of flash memory soon, so we looking for an alternative. I've seen that a bigger G0x1 (STM32G0B1) will be available in the second half of this year. Are there more details available f...

Marco.R by Senior
  • 3755 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.