2021-03-04 4:50 PM
Hi,
I have 50Hz sinewave with 660mVp-pk, should i connect this to SDADC analog input? It can measure negative cycle of the sinewave? i.e. If i configure SDADC as single ended zero reference mode then it can measure negative cycle of the sinewave?
Nandish
Solved! Go to Solution.
2021-03-04 11:18 PM
> If i configure SDADC as single ended zero reference mode then it can measure negative cycle of the sinewave?
No. You have to observe the voltage limits given in datasheet.
JW
2021-03-04 11:18 PM
> If i configure SDADC as single ended zero reference mode then it can measure negative cycle of the sinewave?
No. You have to observe the voltage limits given in datasheet.
JW
2021-03-04 11:40 PM
JW is correct, you cannot measure negative voltages with on-chip means.
You need a dual-supplied opamp to shift the voltage to 0...1320mV - which can amplify the signal by at least factor 2 to make better use of the ADC range.
2021-03-05 2:30 AM
You can bias the ADC input at VREF/2 and capacitive couple the AC input. However as a tip, reconsider the use of the F353 SDADC. Without calibrating each channel, gain is off about 1 % . Calbration must happen with a MUX providing 0.5 ... 0.95 VREF, as VREF will lead to overflow.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.