STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Reset timer output compare output with timer in one pulse mode

I am using an STM32H742 MCU and have a timer with an output connected to the output compare function. The timer is triggered from another timer and set to One Pulse Mode. Basically I want the output to go high and stay high once the compare value is ...

JBerry by Associate III
  • 4537 Views
  • 5 replies
  • 1 kudos

DMA unexpected work on stm32g071

i want to use dma ch2 to response a request of Req_CC3 to load a new value to TIM1 CCR1 or CCR2 . i need dma in some turns but not always so i choose nomal mode. i'd like to know if dma request is  accumulated in stack or somewhere. caus...

rpip.1 by Associate III
  • 1143 Views
  • 1 replies
  • 0 kudos

How to find the address of the BLE advertising device?

I have to extract the RSSI from scanned packet w.r.t to its device address. I got the RSSI but I am unable to get the actual device address. But in the manual they mentioned that"Once the scan parameters are set, the device scanning can be enabled. T...

Kryptons by Associate II
  • 1083 Views
  • 0 replies
  • 0 kudos

Resolved! Is it possible to trigger serially using timers.

For example, there are 3 timers (Timer 1, 2, 3).I want to set like below: Timer 1 : MasterTimer 2 : Slave of Timer1Timer 3 : Slave of Timer2When I checked the waveform after setting similarly to the above, it seemed that timer2 could not trigger time...

SPark.28 by Associate II
  • 1506 Views
  • 3 replies
  • 0 kudos

Resolved! IWDG reset

Hi,I use STM32L496RGT6 with own bootloader. If I start IWDG in bootloader and periodically reset it it is work good. If I jump to application and call HAL_IWDG_Refresh(..), function doesn't refresh IWDG and IWDG reset mcu. I tried call MX_IWDG_Init()...

lorant124 by Associate III
  • 2530 Views
  • 1 replies
  • 0 kudos

'Black Pill' HID gamepad (newbie)

I just bought a 'black pill' STM32F411CE. My goal is to create a HID joystick/gamepad device. While I have been a Software Developer for over 30 years (mostly Windows end-user apps), these boards are completely new to me. So please understand my igno...

CCurl.1 by Associate
  • 1253 Views
  • 0 replies
  • 0 kudos

Resolved! Daylight Saving: The Details?

This is a spiritual followup to this post: https://community.st.com/s/question/0D50X00009XkYuH/rtc-daylight-saving-time-stm32f3-discoverySo I do get which functions to use for daylight saving, and how to BCK bit remembers if I already changed to DST ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.