STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

There is a need to interact with the 3-pin MediaLB bus.

Hey!There is a need to interact with the 3-pin MediaLB bus.I cannot penetrate into it.How the data exchange takes place, what conditions must be observed, how the request and return frame is formed.Perhaps there are examples of working with the bus o...

ALich.1 by Associate
  • 1512 Views
  • 2 replies
  • 0 kudos

SPI modes unclear

Hi everyone,I am working with the SPI in slave mode on an STM32G071 and having some trouble with the different SPI modes. I set both CPOL and CPHA to 0 during initialization: SPI_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX; SPI_InitStruct.Mode...

Fabian21 by Associate III
  • 3224 Views
  • 3 replies
  • 0 kudos

Resolved! Could ADC+DMA brick my mcu?

I was happily developing some ADC+DMA routines for my stm32f205 and suddenly my MCU started to freeze.I am able to connect, erase, and flash binaries with stm32CubeProgrammer trough an ST-link.After erasing multiple times my STM32F205 with stlink and...

0693W000008wIOnQAM.png 0693W000008wIZHQA2.png 0693W000008wIlcQAE.png 0693W000008wIWXQA2.png
Javier1 by Principal
  • 1102 Views
  • 1 replies
  • 0 kudos

STM32G071 write protection, bricked MCU flash

Hello, MCU bricked after I tried to remove write protection. Now when I read the flash it shows only 0xFFFF0080. Read the full description bellow. We are making new project using STM32G071.We use serial communication custom bootloader so we can updat...

0693W000008GRaUQAW.jpg 0693W000008GRfyQAG.jpg
SAlek by Associate II
  • 2344 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.