STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32 Nucleo L476RG

Hi,I'm using a Nucleo L476RG as a master and I want to use it in SPI mode 1, which means the data is transferred in rising edge of the SCLK and data is sampled in falling edge (based on ST documents). Is this the correct configuration for the SPI mod...

0693W000008wbfiQAA.png

Resolved! STM32F410R8 SPI DMA not reading

I've configured the SPI to work with DMA. The microcontroller is sending but is not reading. I have checked the configuration and I cannot see the problem. Can you see something strange in my code.I've tested this code in an STM32F429-DISCO board and...

JPeña.1 by Associate II
  • 1305 Views
  • 3 replies
  • 0 kudos

I can't join.

AADSTS50020: Пользователь�?ка�? учетна�? запи�?ь 'lunin_ser@outlook.com' от по�?тавщика идентификационных данных 'live.com' не �?уще�?твует в арендаторе 'STMicroelectronics' и не может получить до�?туп к приложению '5e3ce6c0-2b1f-4285-8d4b-75ee787734...

SLuni.1 by Associate
  • 1329 Views
  • 2 replies
  • 0 kudos

External clock for STWIN data adquisition

Hello friends of STM. I am new to STM32 MCUs, and I am working on a project using the STWIN. I have another Data Adquisition Card that is programmed to output a clock signal when I send a command or press a button. I would like to datalog the signals...

JQ.2 by Associate
  • 612 Views
  • 0 replies
  • 1 kudos

About Tamper Protection.

Hi all,I'm reading about Tamper Protection on STM32 MCUs.Is this to protect, for example, a device from someone triyng to open the external case?Can you detail some more applications of this feature?

JAlca by Senior
  • 2434 Views
  • 2 replies
  • 1 kudos

Clock configuration when executing program from boot.

I have a question about clock config.Is this a right way to execute program from boot and set clock config like HSE and PLL, then execute program from user app and set clock config again? Actually, there is an error when executing user app.It seems ...

HEhat.1 by Associate II
  • 875 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.