STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[STM32H7] Why is there no spread spectrum functionality?

Hi,as there is apparently no more spread spectrum functionality in the STM32H7 to reduce EMI, is there some counterpart? I heard that the PLL fractional divider might be used for that purpose, but the amount of processor overhead to change the three ...

MaxMax by Associate II
  • 2856 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H743-EVAL2, why battery-backed RAM doesn't hold data?

I start from any simple Cube example, such as UART_Printf,enable access to the backup RAM and write some data.After reset by the reset button or NVIC_System_Reset data in the backup RAM is retained.But after powering off the data is lost.Do I miss so...

Pavel A. by Super User
  • 3288 Views
  • 6 replies
  • 0 kudos

Resolved! Could anyone help me calculate TIM frequency?

Hello everyone,I'm using TIM3 on my Nucleo H745. If it's correct this TIM gets fed from the CPU clock, so it runs at 480MHz. That's what I thought at least.Using these settings;htim3.Init.Prescaler = 48000;htim3.Init.Period = 10000;To my calculations...

Jvan .10 by Associate III
  • 1998 Views
  • 3 replies
  • 0 kudos

How to implement the TIM_IRQHandler when using other classes

I'm trying to make a scheduler and everything seems to be ready, now the final step is add the proper function to the IRQ_Handler. This is where my problem starts. At default this uses a extern tim object from the main.c. I removed it there and put i...

Jvan .10 by Associate III
  • 2493 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.