STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I'd like to use a ST-Link Utility to extract F/W

I'd like to use a ST-Link Utility to extract F/WThe device I'm using is the "STR736FV0T6"and I have ST-LINK/V2 and ULINK2The other day, I had an experience of extracting the one on the STM32F205 device.Isn't STR736 supported?I want to know which JTAG...

HHoja.1 by Associate II
  • 3754 Views
  • 7 replies
  • 0 kudos

Resolved! STM32F429 and STM32F407, the corresponding DMA routines of these two chips.

�?�以直接将STM32F429的DMA例程直接下载到STM32F407中使用�??我这边直接下了进去,�?试了一下,�?�现串�?�没数�?�。​应该是�?对STM32F429的例程修改�?STM32F407版本的例程?如果是�?修改的�?,具体应该修改哪些地方呢?​�?次接触,特�?�请教​感谢�?

Lyang.6 by Associate II
  • 3594 Views
  • 6 replies
  • 1 kudos

About half-duplex communication (Rx frame size is 3)-2

Hello,Is it possible to perform half-duplex communication like the attached document? (I understand that the timing to switch to Rx is tricky.)The Rx frame size is 3 instead of 1.After changing to Rx, can I receive 3 bytes continuously as shown in th...

Connecting PWM output to input on the same board

Good day everyone,At the moment I'm trying to connect a PWM output pin to a PWM input pin on the same board. I'm using a dual core MCU, so both of them are on a different core.I set TIM4 to the M7 and TIM15 to the M4. I enabled the interrupt for TIM1...

0693W000008wfRGQAY.png 0693W000008wfRQQAY.png 0693W000008wfRaQAI.png 0693W000008wfRfQAI.png
Jvan .10 by Associate III
  • 1374 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.