2021-03-11 7:43 AM
2021-03-11 11:52 AM
Hello @Embedded123
Welcome to the STM32 Community =)
It is possible to disable BOOT_CM4 option bit (see "FLASH option bytes" section in the reference manual RM0399)
You can use STM32CubeProgrammer to disable the CM4 in the option bytes.
Imen
2021-03-11 11:59 AM
Hi Imen,
Thank you for your answer.
If I understand well, you are proposing a way to disable the CM4 from booting after a reset/power up?
I have code running on both cores. I'm trying to find a way to reset one from the other. Is there a way to do that?
Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.