STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SPI CPHA affects NSS

I use MCU STM32L462ET6TR. When I set CPHA=1, the NSS signal is always at low. When CPHA=0, NSS signal works normally. There is my initialization code:void MX_SPI1_Init(void) { hspi1.Instance = SPI1; hspi1.Init.Mode = SPI_MODE_MASTER; hspi1.Init...

sdianoff by Associate II
  • 2267 Views
  • 3 replies
  • 0 kudos

stm32f103c8t6 suggest for new design?

Hi there, since Nov. 2020, we have placed some orders to Arrow China, but till now, no one package received, and even no any upate about the orde. ​Please help us with current situation, we start use ST processor since 2010, but now... really sad a...

Xmiao.1 by Associate
  • 1087 Views
  • 1 replies
  • 0 kudos

Resolved! USART3 (PB10, PB11) not working on NUCLEO-G474RE

Hello,I'm working on a NUCLEO-G474RE board (using the LL libraries available on ST site), and I came across an issue, the USART3 available on the PB10 and PB11 is not working. I tried to generate the same code from the CUBEMX as well but unfortunatel...

0693W000008GNhlQAG.png

Write enable QSPI Macronix MX25L51245G

Hi ,I come to you to ask for help with Macronix MX25L51245G interfaced with STM32L476RG. My QSPI is set to 32MHz.Here what I do :QSPI Reset (0x66 - 0x99)SPI Reset (0x66 - 0x99)Wait for WIP = 0 (SPI)Enter in QPI (0x35) 1 lineWait for QUADEN = 1 and WI...

ACHAB.1 by Associate
  • 1557 Views
  • 0 replies
  • 1 kudos

Can't exchange messages FDCAN STM32H743ZI2

Hi, I have two H743ZI2 board. I am trying to send and receive the message with interrupts. When i push the blue button it send the message. But the message is never received.... I already check everything but i can't find the error. I am using a MCP2...

IRodr.2 by Associate II
  • 1391 Views
  • 0 replies
  • 0 kudos

Control the tfmini incoming data.

Hi I am using the tfmini lidar sensor with my nucleo-64 board.but the incoming data is so much fast that i can't control it and is going to error handler.It is a over run.Do anyone has any idea how could i control the burst of data.The link for the l...

Flash download error: Failed to open .sim file| IAR Workbench

Hello Everyone,I'm using STM32H7 family microcontroller and when try to debug the code from IAR Workbench there is a error popup on my screen like " Flash download error: Failed to open file 'Project Folder\EWARM\Project\Exe\ProjectName.sim' ". After...

0693W000005918xQAA.jpg
RLalj.1 by Associate II
  • 4053 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.