STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 GPIO Behavior on Shutdown

I've read through the datasheet and reference manual for STM32L451REI and have been trying to nail down some definitive answers for GPIO behavior upon SHUTDOWN mode. I can't seem to find them, so I'll ask here.In SHUTDOWN MODE:are pullups/pulldowns f...

stm32g031j6m6 NRST as output not working

Hello. Using NRST as an output. Initial state 1. After loading, I switch to 0 and the MCU is rebooted :(. I used options PA0, PA1, PA2. If I use PF2, then the output is constant 1. MCU stm32g031j6m6. On the STM32G0316-DISCO board, the same MPU works ...

V.VIZNIUK by Associate II
  • 1602 Views
  • 3 replies
  • 0 kudos

Using ADC3 when ADC 1 & 2 are running in DMA

I am successfully using a timer and DMA to capture 4096 samples from ADCs 1 & 2 using a master slave configuration on a STM32H747- Disco board.I would really like to simultaneously capture 3 channels. Is it possible to capture samples from ADC 3 usin...

AStew.1 by Associate II
  • 862 Views
  • 0 replies
  • 0 kudos

Stm32H7 DMA ADC Low Bit Resolution

Hello Everyone,I am using the stm32h7 to sample 4 channels from adc1 using the DMA.I am using circular mode with half word size. I start the dma and let it fill up a memory buffer:volatile uint16_t adcInsDMA[4*ADCBLOCKSIZE] = {0};   HAL_StatusTypeDe...

0693W000008y4RNQAY.png
TCash.1 by Associate III
  • 1812 Views
  • 5 replies
  • 0 kudos

Resolved! Blinking LED

Hi all,Just started with bare metal programming of stm32f411re.Uploaded the following code to blink the onboard led of the nucleo board.Code:#include "stm32f4xx.h"         // Device headervoid delayMs(int delay);int main (void){RCC->AHB1ENR |= 1;GPIO...

KRaja.1 by Associate
  • 1875 Views
  • 2 replies
  • 0 kudos

Connecting STM32F7 FMC with SDRAM and 8 bit data bus

When using a 16 bit data bus, the STM32CubeMX generates outputs for FMC_NBL1 and FMC_NBL0 that connect to the SDRAM DQMH and DQML pins. If the STM32CubeMX is configured for an 8 bit data bus, there is no DQM pin generated, although the 8 bit SDRAM h...

MPatt.11 by Associate II
  • 5100 Views
  • 6 replies
  • 0 kudos

STM32H750VB

Hello,I want to ask if it is possible to drive TFT with FMC (Flexible Memory Controller), our TFT has only MCU interfaceI think EMwin has no option for MCU interface at STemWin_CM7_wc16 library.We used same TFT with STM32F207 by using FSMC .If its n...

AKINI by Associate III
  • 862 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.