STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Debugging STM32F769i-disco using openocd and gdb in Linux

Hello ST,I'm trying to launch a debug session for STM32f769i-disco using openocd and gdb in linux. I've install openocd(0.10.0), gdb and gdb-multiarch tools in linux.This is the below log after launching openocd with my board's config file.openocd -f...

Resolved! How to configure a 64 bit quadrature encoder interface

I'm currently using TIM2 on an STM32F373 as a 32bit quadrature encoder interface, however I need to extend this to 64 bits. Can I cascade a second 32bit counter (e.g. TIM5) as a slave whilst still maintaining the ability to count up & down ? Thanks

RParf.1 by Associate II
  • 3757 Views
  • 7 replies
  • 0 kudos

Resolved! Right edge aligned PWM

I've edited this post to make it more useful to others.We are well into development of a board at work using an STM32F072RBT6 MCU. I just wrote a quick from scratch test using a NUCLEO-F072RB board to verify things. I'm not sure of the exact problem,...

SPetr.6 by Associate III
  • 3838 Views
  • 6 replies
  • 0 kudos

MCU starts code if I do a hardware reset!

Hello,I'm working with STM32F427VIT6 microcontroller. BOOT0 is connected to GND through 10K resistor. The NRST state is high.My problem is when I power up the board, the microcontroller code execution seems to not start. The execution only starts if ...

BS.2 by Associate
  • 3034 Views
  • 3 replies
  • 0 kudos

STM32G474 dual bank feature seems not working.

My application is running in Bank1 and I program new firmware binary file to bank2 via USB and toggle the bank(set BFB2), it does not start . When I check the binary file generated by cubeIDE and the binary file written to bank2(using cubeprogrammer)...

HYe_i.1 by Associate
  • 1217 Views
  • 1 replies
  • 0 kudos

STM32G474 ADC in continuous regular scanning mode with injection fails due to injection channels being internally tied to ground

I am trying to set up my NUCLEO-G474RE board to perform ADC regular scanning mode using DMA with 4 channels and also discontinuous injection with 2 channels as shown below.But when I run my code the injected channels always return zero or one, even i...

0693W000007EvA4QAK.jpg 0693W000007EvFxQAK.jpg 0693W000007EvHyQAK.jpg
CHossack by Associate III
  • 2615 Views
  • 2 replies
  • 0 kudos

Resolved! stm32h747: XIP from external SDRAM

Is it possible to run the firmware from an external SDRAM?There is an example for h750, but it does not work with h747.I go to the address I need, but I get a hardfault into bootloader for first command into external sdram

0693W000008zkr0QAA.jpg
VLesc.1 by Associate
  • 1254 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.