2021-04-16 2:30 AM
Is it possible to run the firmware from an external SDRAM?
There is an example for h750, but it does not work with h747.
I go to the address I need, but I get a hardfault into bootloader for first command into external sdram
Solved! Go to Solution.
2021-04-16 7:28 AM
Hello
External SDRAM is execute disabled by default.
The MPU can override the default memory access.
Need to configure SDRAM region in MPU with XN bit at RASR register, disabled.
2021-04-16 7:28 AM
Hello
External SDRAM is execute disabled by default.
The MPU can override the default memory access.
Need to configure SDRAM region in MPU with XN bit at RASR register, disabled.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.