STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F105 DFU Bootloader Grief

Hi all.I'm new to STM, but have been designing and making embedded MCU products for over ten years.I was drawn to the STM32F105 series because of the USB DFU, to allow for field updates for prospective customers to update a product we're developing. ...

Tad_E by Associate II
  • 2537 Views
  • 6 replies
  • 0 kudos

Resolved! In Shutdown, how is RTC powered?

While I was experimenting with the 'L476 Disco, the RM wording goes across multiple families, so it may be relevant to most/all of them. In particular, for Shutdown mode (which is supposedly the lowest-VDD-consumption mode), the RM says: What does "...

Clipboard01.png

Resolved! Microcontroller with some kind of audio I/O capability ?

Split from WiFi or WiFi+BT modules architecture and parts recommendations as that's really a separate question!Thank you @Andrew Neil I didn’t explain myself very clearly. The part I’m mainly interested in is the audio side — specifically, a microcon...

Ricko by Senior III
  • 625 Views
  • 7 replies
  • 9 kudos

Resolved! STM32G071GBU6 top marking

(I tried to submit a ticket but the system seems broken, giving an obscure error about an incorrect zip code).I need to confirm which version of STM32 is placed on a board. There are two versions, GP and PD. The datasheet does not really specify how ...

pmillett_1-1776873894947.png STM32.jpg
pmillett by Associate
  • 233 Views
  • 2 replies
  • 0 kudos

STM32H753 Current Comsumption

Hello, in the STM32H753xI datasheet, Table 11, "Total current into sum of all VDD power lines (620mA)," is the voltage condition VDD = 3.3V? I would also like to know the current at VDD = 1.8V.

Koichi-H by Associate
  • 355 Views
  • 4 replies
  • 6 kudos

STM32C0 not driving CAN bus

STM32C092CCT6 : TCAN1463-Q1: TXD Dominant but No CAN Output — Bit0 Errors, nFAULT OK, Normal Mode Confirmed Hello everyone,I am facing an issue where the CAN transceiver (TCAN1463-Q1) does not drive the CAN bus even though the STM32 FDCAN peripheral ...

STM32G070RBT6 with external pull-up resistor having weird voltage level

Post edited by a ST moderator: 1- Translate the text to English. 2- Update the title to be more concise. 3- Update the label.   我在使用STM32G070系列芯片时,外部电阻上拉到3.3V,接入STM32芯片后测量,发现GPIOA 15 和GPIO A8两个引脚是0.9V的电压,为什么? Translation: "When using the STM32G070 se...

AAApink by Associate
  • 218 Views
  • 1 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.