2026-04-22 9:05 AM
(I tried to submit a ticket but the system seems broken, giving an obscure error about an incorrect zip code).
I need to confirm which version of STM32 is placed on a board. There are two versions, GP and PD. The datasheet does not really specify how the top marking is different for the two versions.
Any ideas?
Thanks, Pete
Solved! Go to Solution.
2026-04-22 9:32 AM
Welcome @pmillett, to the community!
The two versions are marked as follows:
So, the device on your photo is a STM32G071GBU6 without N.
BTW: The marking is also shown on the packaging label.
Hope that helps?
Regards
/Peter
2026-04-22 9:32 AM
Welcome @pmillett, to the community!
The two versions are marked as follows:
So, the device on your photo is a STM32G071GBU6 without N.
BTW: The marking is also shown on the packaging label.
Hope that helps?
Regards
/Peter
2026-04-22 1:06 PM
Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.