2026-04-21 8:44 PM - last edited on 2026-04-22 1:19 AM by mƎALLEm
Post edited by a ST moderator:
1- Translate the text to English.
2- Update the title to be more concise.
3- Update the label.
我在使用STM32G070系列芯片时,外部电阻上拉到3.3V,接入STM32芯片后测量,发现GPIOA 15 和GPIO A8两个引脚是0.9V的电压,为什么?
Translation:
"When using the STM32G070 series chip, I pulled the external resistor up to 3.3V. After connecting it to the STM32 chip, I measured the voltage on the GPIOA 15 and GPIO A8 pins and found that they were 0.9V. Why is that?"
2026-04-22 1:01 AM
Hello @AAApink and welcome to the community;
The language of this community is English, please look at How to write your question to maximize your chance... - STMicroelectronics Community.
@AAApink wrote:
我在使用STM32G070系列芯片时,外部电阻上拉到3.3V,接入STM32芯片后测量,发现GPIOA 15 和GPIO A8两个引脚是0.9V的电压,为什么?
Translation: "When using the STM32G070 series chip, I pulled the external resistor up to 3.3V. After connecting it to the STM32 chip, I measured the voltage on the GPIOA 15 and GPIO A8 pins and found that they were 0.9V. Why is that?"
PA15 or PB15?
For PA8 pin, upon reset, a pull-down resistor might be present on PA8, PB15, PD0, or PD2, depending on the voltage level on PA9/PC6, PA10/PB0, PD1, and PD3, respectively. In order to disable this resistor, strobe the UCPDx_STROBE bit of the SYSCFG_CFGR1 register during start-up sequence, please look at Datasheet - STM32G070CB/KB/RB - Arm<Sup>® </Sup>Cortex<Sup>®</Sup>-M0+ 32-bit MCU, 128 KB Flash, 36 KB RAM, 4x USART, timers, ADC, comm. I/Fs, 2.0-3.6 V.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.