Is there a new STM32F427 DS or not?
This:downloads this:So, is there a new DS, dated 13.May 2021, or not?JW
Ask questions, find answers, and share insights on STM32 products and their technical features.
This:downloads this:So, is there a new DS, dated 13.May 2021, or not?JW
I am looking for STM32F072RB part no but currently it is out of stock and not available anywhere. Can somebody provide alternative part no which is available easily.Please share the source details .Any help would be helpful. Thank you.
I need to fix something in a project that I didn't program.The problem occures (sometimes) after the product is restarted 24 hours after we remve it from the USB.The project uses HAL_PWR_EnterSTANDBYMode to enter the Low level mode, but I don't see a...
Hi all,I'm currently working on a STM32H743. The idea is to use a SAI peripherals to read an Audio stream:The SAI is set to be a Master receive with a circular buffer and a DMAThe issue is that as soon as the HAL_SAI_Receive_DMA is called, then the c...
I need to take 10 samples (10 Hz) per second. How can I set ADC configurations on CubeMX. I use the lowest sampling time (2.5 cycles), but the values I convert and use in ADC change very quickly.Thanks for helps.
Hi - I'm learning DMA, and am having some trouble. (L4, but this applies to most/all STM32s)For SPI, the RM States this:"To close communication it is mandatory to follow these steps in order: 1. Disable DMA streams for Tx and Rx in the DMA registers,...
i am using stm32h743 microcontroller ,in this i am working on the uart in dma mode for receiver i am using circular mode and for transmitter i am using normal mode. the communication is working in the first time , when i am trying to transmit the dat...
We are looking for STM32F072RBT6 part but it is out of stock at many places. Can anyone suggest source for the same IC.Any alternative part suggestion would also be helpful. Thank you in advance.I am sorry if this is not the right place to post this ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.