STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U575 OTG_FS host suspend and remote wakeup failure

I am trying to implement an application with USB CDC-ECM host capabilities. As a bring up setup, I configured two STM32 boards:1) STM32U5G9J-DK2 board, configured as a CDC-ECM device, using USBX.2) STM32U575I-EV, configured as a CDC-ECM host, using U...

talk by Associate II
  • 1707 Views
  • 6 replies
  • 2 kudos

STM32H725 TIM5 issue

I am using one of the 32 bit timers to measure intervals for fault protection on a HV pulse modulator.  I have an interrupt on EXTI that captures both leading and trailing edges of the command pulse.   In the service routine, I simply store the lates...

JCase.1 by Associate III
  • 661 Views
  • 1 replies
  • 0 kudos

STM32H735 wake from standby

My simple program to test wake from standby with PC13/Wakeup_pin4 is working.  I use the pushbutton on this pin as an EXTI and had to add the GPIO_DeInit before setting the pin as an input without EXTI.The same code does not work in my larger program...

Ian_CP by Associate II
  • 934 Views
  • 5 replies
  • 0 kudos

Resolved! Any STM32 with Split Power SPI Domains (1.8V & 3.3V IOs) ?

I’m working on a design where I need to communicate with two SPI devices that operate at different logic levels:1) A sensor running at 1.8v logic (need SPI + 2 other lines, all at 1.8v) 2) Everything else on my board, preferably running at 3.3v, I wi...

sc123 by Associate
  • 1175 Views
  • 4 replies
  • 1 kudos

Resolved! STM32L011G4U6TR build Error: Flash Overflow

Hello All, I am using STM32L011G4U6TR for one of my application development. I have written a code where I am using,11 GPIO, 1 UART and Internat EEProm.When I am building the code in I am getting below Error and not able to load the Application on ST...

Shiv09_0-1752586521299.png
Shiv09 by Senior
  • 1144 Views
  • 7 replies
  • 6 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.